Change screens based on values

Display different screens based on a variable value or tag value. For example, display a screen when a tank surpasses a certain level.
At runtime, the sample application:
  • Updates the controller tag or model variable value when user selects a different screen
  • Updates the displayed screen when the controller tag or model variable changes
Application example
NOTE:
Download a sample project:
ChangeScreens.zip
Prerequisites
  1. To develop the project
  2. Arrange the interface elements.
  3. Save the project.
Application design example
Select
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a target device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal