Configure the authentication mode

Change the default authentication mode to allow local users and domain users to log on at runtime.
Prerequisites
To allow Active Directory users to authenticate, either:
  • Obtain the Active Directory domain name and server address.
  • Ensure that the
    Windows
    client is joined to the Active Directory domain.
To allow LDAP users to authenticate, obtain:
  • LDAP server address
  • Base64 CA certificate file exported from the Active Directory server or from a computer in the domain
TIP:
FactoryTalk Optix Studio
does not support LDAP over SSL (LDAPS).
  1. To configure the authentication mode
  2. In
    Project view
    , select the root node.
  3. In
    Properties
    , expand
    Authentication
    , and then in
    Authentication mode
    , select an authentication type:
    • Model only
      . Users created in
      FactoryTalk Optix Studio
      .
    • Local only
      . Local machine users.
    • Domain only
      . Active Directory and LDAP users.
    • Domain and local
      . Active Directory, LDAP, and local machine users.
    • Domain, local, and model
      . Active Directory and LDAP users, local machine users, and users created in
      FactoryTalk Optix Studio
      .
    • OAuth 2.0
      . Users authorized with the OAuth 2.0 protocol. 
  4. Configure properties for the selected authentication mode.
    For more information, see Authentication properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal