Create an enumeration

Create an enumeration object and define enumeration members in the editor.
  1. Right-click a node to contain the enumeration and select
    New
    All
    Data type
    .
  2. Select
    Enumeration
    and choose
    Select
    .
    Enumeration
    #
    appears under the node.
  3. In
    Project view
    , double-click
    Enumeration
    #
    .
    Enumeration editor displays in the editor.
  4. In the editor, manage the enumeration members:
    • To add a member, select
      Add
      and complete:
      • Value
        . Enumeration member value. Value is generally a consecutive integer.
      • Display name
        . Name of the enumeration member.
      • Description
        . Additional information about the enumeration member.
    • To edit a
      Value
      ,
      Display name
      , or
      Description
      , double-click the corresponding cell and enter a new value.
    • To remove a member, select a cell in the corresponding row and select
      Delete
      .
  5. (optional) In
    Properties
    , select
    Add
    , select
    Display name
    , and enter the display name.
  6. (optional) In
    Properties
    , select
    Add
    , select
    Description
    , and enter the description.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal