Certificate errors

Certificate errors may display when using the web browser object.
Certificate errors that are ignored at runtime when
Ignore invalid CA errors
is set to
True
. For more information, see Configure a web browser.
Certificate errors
Error
Description
CertificateAuthorityInvalid
Certificate not signed by a trusted CA
Certificate errors listed in
Certificate error
. To ignore the errors, select
Accept the risk and continue
at runtime.
Certificate errors
Error
Description
SslPinnedKeyNotInCertificateChain
Certificate does not match the built-in public keys pinned for the host name
CertificateCommonNameInvalid
Certificate common name does not match host name
CertificateDateInvalid
Certificate is not valid at the current date and time
CertificateAuthorityInvalid
Certificate not signed by a trusted CA
CertificateContainsErrors
Certificate contains errors
CertificateNoRevocationMechanism
Unable to determine if the certificate is revoked
CertificateUnableToCheckRevocation
Unable to get revocation information for the certificate
CertificateRevoked
Revoked certificate
CertificateInvalid
Invalid certificate
CertificateWeakSignatureAlgorithm
Certificate signed with a weak signature algorithm
CertificateNonUniqueName
Certificate host name is not unique
CertificateWeakKey
Certificate contains a weak key
CertificateNameConstraintViolation
Certificate claimed DNS names violate name constraints
CertificateValidityTooLong
Too long certificate validity period
CertificateTransparencyRequired
Unable to get required certificate transparency information from the server
CertificateKnownInterceptionBlocked
Certificate known for interception by an entity other than the device owner
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal