Create an Advanced SVG Image

Prerequisites
Download the star_rectangle.svg image.
  1. To create an Advanced SVG Image
  2. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Drawings
    Advanced SVG Image
    .
  3. Double-click
    MainWindow (type)
    .
  4. Double-click the empty image
    Image placeholder
    on the canvas.
  5. Select
    Import file(s)
    and in
    Import file(s)
    , select the file to import and then choose
    Select
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal