FactoryTalk Optix runtime modes

When you deploy an application, the mode in which
FactoryTalk Optix
runs depends on how
FactoryTalk Optix
Update Server is configured upon installation.
The two
FactoryTalk Optix
modes are:
  • FactoryTalk Optix running as an application mode.
    When FactoryTalk Optix is running as an application, the deployed application is accessible with the native presentation engine and web presentation engine. This mode is generally used by a local user logged onto the device or accessing the HMI and any remote users connecting from a web client if the web presentation was added.
  • FactoryTalk Optix running as a service mode.
    In this mode,
    FactoryTalk Optix
    runs the deployed application as a Windows service. The service starts when the runtime device starts and automatically runs the deployed application. This mode uses the
    Web Presentation Engine
    that you must add to
    Project view
    . Use this mode to interact with the application using the web browser of any device that can access the runtime device through an Ethernet IP address. Without a
    Web Presentation Engine
    , the application still runs without displaying on a user interface. This mode is generally used when the application has no user interface, such as a data gateway.
    TIP: The
    Native Presentation Engine
    is not supported in
    FactoryTalk Optix
    Runtime as a service mode.
TIP:
FactoryTalk Optix Applications
that use Runtime as a service mode are deployed to C:\ProgramData\Rockwell Automation\FactoryTalk Optix\FTOptixRuntimeService.
To use either runtime mode, install the FactoryTalk Optix Runtime Tools on the runtime device.See the
FactoryTalk Optix Installation Guide
. You can customize the installation to install FactoryTalk Optix runtime as a service. If you do not install FactoryTalk Optix runtime as a service, it installs as an application by default.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal