Graphic objects

Use predefined graphic objects to add visual components to
FactoryTalk Optix Applications
. Use Presentation Engines to display the UI at runtime on different viewports.
FactoryTalk Optix Studio
includes predefined graphic objects to add and arrange in the visual editor. See Predefined graphic objects and Editor.
In
Project view
and in the editor, create, duplicate, edit, and set the properties of graphic object instances and graphic object types. See Manage graphic objects and Graphic objects layout.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal