Options

The top title bar contains the
Options
configuration button, access to the help, and the user sign-in.
To configure options
, select
FactoryTalk Optix Studio Options
. boolean : no
TIP:
If you select the drop-down arrow next to the icon, select
FactoryTalk Optix Studio
Options
.
FactoryTalk Optix Studio
Options
Item
Description
Remarks
Language
The language used in the interface. Select:
  • en-US: Standard American English
  • it-IT: Standard Italian
  • de-DE: Standard German
After changing a language option, restart
FactoryTalk Optix Studio
.
Advanced mode
Activates the advanced log messages display in the log panel.
For more information on log panel configuration see Module log level configuration.
Show feature previews
Activates features under development.
These features are denoted by (preview). Do not use these features in production systems.
Preferred code editor
Set the default code editor for use with the any NetLogic C# code.
Select:
  • Visual Studio
  • Visual Studio Code
  • System-defined
    Uses the code editor installed on your system.
Preferred physical length unit
Set the default unit of measurement for physical lengths.
Select:
  • Automatic
  • mm
    (millimeters)
  • cm
    (centimeters)
  • in
    (inches)
Source Control User Configuration
Settings used when a project is stored in a source control repository
User Name
User name of the logged in user account.
This name displays in the project history for any changes made during their session.
User Email
Email account of the logged in user account.
Specify the email using the user name and domain. Example: someone@example.com
Update
FactoryTalk Optix Studio
Links to the download page to download updates to
FactoryTalk Optix Studio
and the runtime tools.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal