About the FactoryTalk Linx Redundancy Module Configuration Tool
FactoryTalk® Linx
Redundancy Module Configuration Tool is an extension
module that enables online operations and configuration of 1756 ControlLogix®
Redundancy Modules, including 1756-RM2 and 1756-RM3. This
tool is launched through the FactoryTalk Linx
Network Browser.FactoryTalk Linx
Redundancy Module Configuration Tool uses FactoryTalk® Audit
logging to create audit messages for each action performed
on the redundancy module.Access to
FactoryTalk Linx
Redundancy Module Configuration Tool is controlled by
FactoryTalk® Security
. You must have the Open Device Configuration
permission to access the tool.
TIP:
To configure the
Open Device Configuration
permission, open FactoryTalk® Administration Console
, and then go to System > Policies > Product
Policies > FactoryTalk Linx > Feature Security
.To launch
FactoryTalk Linx
Redundancy Module Configuration Tool, locate a 1756 ControlLogix Redundancy Module in the FactoryTalk Linx
Network Browser topology view, right-click the module, and then select Device Configuration
.
TIP:
- The tool supports 1756-RM2 modules with firmware revision 20.010 or later.
- The tool must be installed on the same computer as theFactoryTalk LinxNetwork Browser for this option to be available.
Rockwell Automation®
recognizes that some of the terms that are currently used
in our industry and in this publication are not in alignment with the movement toward
inclusive language in technology. We are proactively collaborating with industry peers to
find alternatives to such terms and making changes to our products and content. Please
excuse the use of such terms in our content while we implement these changes.Provide Feedback