The MQTT interface is not working
- Verify Windows Local Service access to the certificate files.
- Verify that the certificate has not expired.
- Verify that the host information in the certificate matches the client computer.
- Verify that the client ID is unique within the broker.
- Verify the broker is running.
- Verify that the host information in the certificate matches the client computer.
- Verify that the client ID is unique within the broker.
- Verify the client dataset's topic name syntax when connection meets problems.
- Verify the client subscribes to the correct topic name, not the dataset name, from FactoryTalk Linx Gateway’s MQTT interface.
- Verify the firewall on the computer with the broker has the broker’s TCP port open.
Provide Feedback