Search
FactoryTalk Linx Gateway Help
FactoryTalk Diagnostics event messages for FactoryTalk Linx Gateway OPC UA Server
In this section:
OPC UA common status codes
FactoryTalk Linx Gateway OPC UA Server obtained the product activation = 'x', scope = 'y', type = 'z'.
FactoryTalk Linx Gateway OPC UA Server has started.
FactoryTalk Linx Gateway OPC UA Server has stopped.
The configuration file does not exist. Use the FactoryTalk Linx Gateway Configuration software to reconfigure the FactoryTalk Linx Gateway OPC UA Server.
The loading service configuration was successful.
Endpoint 'x' is open and available.
Failed to enable endpoint 'x'. The reason is 'y'. Review the service configuration in the configuration tool and verify the endpoint port isn't used by another endpoint or is blocked by the firewall.
The FactoryTalk Linx Gateway UA service version 'x' successfully connected to the live data server via scope 'y'.
The FactoryTalk Linx Gateway OPC UA Server version 'x' failed to connect to the live data server via scope 'y'. Check the selected scope and live data service status in the configuration tool.
The client 'x', 'y' connected to FactoryTalk Linx Gateway OPC UA Server from endpoint 'z', security mode 'x1', and security policy 'y1'.
The client 'x', 'y' failed to connect to the FactoryTalk Linx Gateway OPC UA Server from endpoint 'z', security mode 'x1', and security policy 'y1'. The reason is 'z1'.
The client 'x', 'y' closed a connection to the FactoryTalk Linx Gateway OPC UA Server from endpoint 'z', security mode 'x1', and security policy 'y1'.
Failed to process the request from client 'x', 'y' to read 'z' tag values. The reason is 'x1'.
Failed to process the request from client 'x', 'y' to create a subscription. The reason is 'z'.
Failed to process the request from client 'x', 'y' to delete a subscription. The reason is 'z'.
Failed to process the request from client 'x', 'y' to monitor 'z' tags. The reason is 'x1'.
Failed to process the request from client 'x', 'y' to delete 'z' monitored tags. The reason is 'x1'..
Failed to process the request from client 'x', 'y' to write values to 'z' tags. The reason is 'x1'.
The FactoryTalk Linx Gateway OPC UA Server failed to add item 'x' because the maximum number of items ('y') has been reached.
The FactoryTalk Linx Gateway OPC UA Server failed to connect to the client because the server has reached its limit of connections.
The tag 'x' value has been changed to 'y' based on the request by user 'z' from OPC UA client 'x1', 'y1'.
There are problems with the service configuration. Use FactoryTalk Linx Gateway Configuration to reconfigure the FactoryTalk Linx Gateway OPC UA Server.
Troubleshoot FactoryTalk Linx Gateway
OPC UA common status codes
FactoryTalk Linx Gateway OPC UA Server obtained the product activation = 'x', scope = 'y', type = 'z'.
FactoryTalk Linx Gateway OPC UA Server has started.
FactoryTalk Linx Gateway OPC UA Server has stopped.
The configuration file does not exist. Use the FactoryTalk Linx Gateway Configuration software to reconfigure the FactoryTalk Linx Gateway OPC UA Server.
The loading service configuration was successful.
Endpoint 'x' is open and available.
Failed to enable endpoint 'x'. The reason is 'y'. Review the service configuration in the configuration tool and verify the endpoint port isn't used by another endpoint or is blocked by the firewall.
The FactoryTalk Linx Gateway UA service version 'x' successfully connected to the live data server via scope 'y'.
The FactoryTalk Linx Gateway OPC UA Server version 'x' failed to connect to the live data server via scope 'y'. Check the selected scope and live data service status in the configuration tool.
The client 'x', 'y' connected to FactoryTalk Linx Gateway OPC UA Server from endpoint 'z', security mode 'x1', and security policy 'y1'.
The client 'x', 'y' failed to connect to the FactoryTalk Linx Gateway OPC UA Server from endpoint 'z', security mode 'x1', and security policy 'y1'. The reason is 'z1'.
The client 'x', 'y' closed a connection to the FactoryTalk Linx Gateway OPC UA Server from endpoint 'z', security mode 'x1', and security policy 'y1'.
Failed to process the request from client 'x', 'y' to read 'z' tag values. The reason is 'x1'.
Failed to process the request from client 'x', 'y' to create a subscription. The reason is 'z'.
Failed to process the request from client 'x', 'y' to delete a subscription. The reason is 'z'.
Failed to process the request from client 'x', 'y' to monitor 'z' tags. The reason is 'x1'.
Failed to process the request from client 'x', 'y' to delete 'z' monitored tags. The reason is 'x1'..
Failed to process the request from client 'x', 'y' to write values to 'z' tags. The reason is 'x1'.
The FactoryTalk Linx Gateway OPC UA Server failed to add item 'x' because the maximum number of items ('y') has been reached.
The FactoryTalk Linx Gateway OPC UA Server failed to connect to the client because the server has reached its limit of connections.
The tag 'x' value has been changed to 'y' based on the request by user 'z' from OPC UA client 'x1', 'y1'.
There are problems with the service configuration. Use FactoryTalk Linx Gateway Configuration to reconfigure the FactoryTalk Linx Gateway OPC UA Server.
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal