Excel RTD formula sample
Use these formulas to read tag values under different options.
On the
Server Configuration
tab, under Excel RTD Interface
,- If you selectFolders with scalar data, the RTD formula could be:=RTD("FTLinxGatewayRTD","","[ShortcutName]TagName",1000,0,"")Example:=RTD("FTLinxGatewayRTD","","[ShortcutName]Tag1",1000,0,"")=RTD("FTLinxGatewayRTD","","[ShortcutName]Program:MainProgram.l_BoolArray1[006]",1000,0,"")=RTD("FTLinxGatewayRTD","","area::[ShortcutName]Program:MainProgram.l_BoolArray1[006]",1000,0,"")=RTD("FTLinxGatewayRTD","","area:FactoryTalk Linx2:[ShortcutName]Program:MainProgram.l_BoolArray1[006]",1000,0,"")=RTD("FTLinxGatewayRTD",""," :FactoryTalk Linx2:[ShortcutName]Program:MainProgram.l_BoolArray1[006]",1000,0,"")=RTD("FTLinxGatewayRTD","","[ShortcutName]StructTag.Element",1000,0,"")=RTD("FTLinxGatewayRTD","","[ShortcutName]Program:MainProgram.StructTag.Element",1000,0,"")
- If you selectCustom namespace, the RTD formula could be:=RTD("FTLinxGatewayRTD","","[NamespaceName]TagName",1000,0,"")Example:=RTD("FTLinxGatewayRTD","","[Namespace_01]Tag1",1000,0,"")
Provide Feedback