MQTT client properties
The following table shows the MQTT client properties.
Field | Description |
|---|---|
Name | Enters the MQTT client name. |
MQTT Broker Address | Enters the IP address or host name of the broker. |
Port | Enters a broker's port. |
Client ID | Edits or regenerate the client ID. The client ID is used to identify the client for a broker. The client ID must be unique within the broker. |
Status | Views the connection status between the client and broker. |
SSL/TLS | Enables or disables secure communication between the client and broker. Make sure that the broker also supports this security protocol.
|
User Authentication | Provides the username and password to the broker authentication. Make sure that the user credentials are enabled in the broker. |
Maximum Number of Messages to Cache | Specifies the maximum number of messages that you want to cache when the network
disconnects.
IMPORTANT:
If the value is too large, the cache
will grow larger than the available memory space. For more information, see
Cache undelivered messages.
|
Strategy to Cache Message | Selects the method to cache messages.
|
Provide Feedback