Add a dataset
Follow these steps to add a dataset within a MQTT client.
Add a dataset
- On the left pane of FactoryTalk Linx Gateway Configuration, expandMQTT, and then select an MQTT client.
- Select
, and then select PublisherorSubscriber.You can back up or restore the dataset when selecting the node.
Provide Feedback