Maintenance
Once the FactoryTalk system is set up, use the following software to maintain it.
- FactoryTalk Live Data Test ClientFactoryTalk Live Data Test Client can monitor each data item individually or as part of a custom group. Activate, deactivate, or change the read and write settings of data items and groups to verify their values are correctly transferred across the network. For more information, seeFactoryTalk Live Data Test Client HelpinFactoryTalk Services Platform Help.
- FactoryTalk DiagnosticsFactoryTalk Diagnostics records activity, status, warning, and error messages generated during the design, management, and operation of a FactoryTalk system.The FactoryTalk Diagnostics service includes a Diagnostics Setup editor, a Diagnostics Viewer, and a local log on each computer where the FactoryTalk Services Platform is installed. Other custom logging destinations are also available. For example, the FactoryTalk AssetCentre software product provides customized FactoryTalk audit logs.To set up options for logging destinations and to filter the types of messages logged on the local computer, useDiagnostics Setup.To review diagnostics messages, use theDiagnostics Viewer. Diagnostics Viewer can be used to view both local messages and messages retrieved and merged from logs on multiple computers.For more information, seeFactoryTalk Diagnostics Setup HelpandFactoryTalk Diagnostics Viewer Help.
- FactoryTalk Diagnostics Counter MonitorFactoryTalk Diagnostics Counter Monitor provides the ability to check the status of tags and to monitor the runtime values of counters and strings that are made available by network clients for diagnostic purposes. For more information, seeFactoryTalk Diagnostics Counter Monitor Help.
- FactoryTalk UpdaterFactoryTalk Updater Agent collects information and activation license data from the Rockwell Automation software installed on the computer. It is the default functionality installed with most Rockwell Automation software. For more information, seeFactoryTalk Updater Help.
Provide Feedback