Considerations when changing the workstation hostname

To ensure system functionality after changing the hostname,
  • Verify the address on
    Endpoints
    of
    OPC UA Server
    .
  • Regenerate the outgoing certificate.
    The OPC UA client must trust the new certificate.
  • Change the host information of the MQTT certificate configuration if necessary.
  • Verify the hostname of the FactoryTalk Linx server and OPC UA server if you also use them on the same computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal