FactoryTalk Linx Data Bridge
FactoryTalk® Linx Data Bridge synchronizes data between
FactoryTalk® Live Data
servers that include FactoryTalk® Linx
, FactoryTalk®
Resource and Status, OPC®
UA, OPC
DA, and
FactoryTalk® View Site Edition (SE)
HMI tags. This can be used between devices and servers
in a FactoryTalk®
application that may not be compatible.When source tag values or timestamps change on a server or device,
FactoryTalk Linx Data Bridge
replicates the values or timestamps to the destination tag on
another server or device. Optional quality and timestamp tags provide metadata about the tag
values.FactoryTalk Linx Data Bridge
supports:- FactoryTalk® Linxdevices
- RSLinx® Classicdevices
- OPCUA servers that support subscriptions
- OPCDA servers
- FactoryTalk View SEHMI tags
The performances of design time tag browsing and runtime tag value updates are dependent on:
- Source tag device or server capabilities
- Destination tag device or server capabilities
- FactoryTalk Linx Data Bridgehost computer capabilities
- Network design and traffic
For best performance, ensure source, destination, and . Connect all devices using a 100 MB or higher Ethernet network.
FactoryTalk Linx Data Bridge
host devices meet the system requirements listed in FactoryTalk Linx Data Bridge
Release Notes Rockwell Automation®
recognizes that some of the terms that are currently used
in our industry and in this publication are not in alignment with the movement toward
inclusive language in technology. We are proactively collaborating with industry peers to
find alternatives to such terms and making changes to our products and content. Please
excuse the use of such terms in our content while we implement these changes.Provide Feedback