Zoom in or out

The zoom feature allows you to zoom in or out on the trend for detailed analyses.
  • To zoom in on the trend with the toolbox:
    • Select
      Zoom
      (Zoom) and press the left mouse button to select a particular time period to zoom in.
    • Select
      Zoom Back
      (Zoom back) to roll back the trend to the last view.
    • Select
      Zoom Reset
      (Zoom reset) to reset the trend to the original view.
  • To zoom in or out the trend without a toolbox:
    • Scroll the mouse wheel up or down to zoom in or out.
    • Put two fingers on the touch screen and move them apart to zoom in and together to zoom out.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal