Edit trend properties
Only users assigned the role of Administrator can view, edit, and save the trend
properties.
To edit trend properties
- Select the trend that you want to edit:
- To edit the trend properties underPrivateorPublic, select
on the user node. - To edit the trend properties underOrphan Trends, select
on the Orphan Trendsnode.
- On theTrend propertiespage, edit the trends as needed.
- Trend Name: Displays all trends listed under this node. The trend name must have 32 characters or less and can only include numbers, letters, and special characters of hyphens (-) and underscores (_).
- Trend Description: Displays the saved trend description. The trend description must have 128 characters or less and can only include numbers, letters, and special characters of hyphens (-) and underscores (_).
- Access Level: Displays the access level of Private or Public.
- Trend Owner: Chooses to change the trend owner to another user.
TIP: To filter and sort trend by Trend Name, Trend Description, Access Level, and Trend Owner, select the arrow and
next to these headers. - SelectSave.
Provide Feedback