Use Y cursors
When the Y cursor is enabled, two horizontal cursors that slide along the Y-axis will be displayed. Each cursor can be operated individually. You can also use the X-axis cursor with the Y-axis cursor.
Cursors:
- Can be used while zooming in on data.
- Allow panning of data.
- Display values of data points that touch the cursor.
To use Y cursors
- On the WebTrend toolbar, selectY Cursors(
). - Drag each cursor up or down on the plot surface. The following information is displayed:
- Data point values for each tag at the cursor location.
- Date and time display for each cursor location.
Provide Feedback