Use X cursors
When the X cursor is enabled, two vertical cursors that slide along the X-axis display. Each cursor can be operated individually. You can also use the X-axis cursor with the Y-axis cursor. This feature is useful when you stack the Y-axis so you can quickly see the values for a point in time for all tags at once and compare those values.
Cursors:
- Can be used while zooming in on data.
- Allow panning of data.
- Display values of data points that touch the cursor.
To use X cursors
- On the WebTrend toolbar, selectX Cursors(
). - Drag each cursor left or right on the plot surface. The following information is displayed:
- Data point values for each tag at the cursor location.
- Date and time display for each cursor location.
Provide Feedback