Select time bar

The trend displays the tag value over a period of time or in real time. The X-axis of the trend always represents time. There are two time modes:
Absolute
and
Relative
. In
Absolute
mode, you select specific dates and times for the start and end of the time period. The start time must be earlier than the end time. In
Relative
mode, you select a typical time period from the dropdown list, such as the last 5 minutes, or the last 1 hour. When a trend is published using a Relative time period, it always retrieves data relative to the present time.
Switch to Live mode by toggling the Live Mode button on the toolbar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal