The following is an overview of the Historian WebTrend interface.
Historian WebTrend interface overview
Historian WebTrend interface overview
Item
Name
Description
1
Toolbar
Displays the commonly used commands, such as Live Mode (), Grid (), and Y Stack ().
2
Time Bar
Provides options to select a time period using absolute or relative time.
When using absolute time, you select specific dates and times for the start and end of the time period. The time difference will be calculated and displayed next to the end time picker. When using relative time, you select a typical time period, such as the last 5 minutes or the last 1 hour.
3
Data Source
Displays Asset Framework and Data Archive from the
FactoryTalk Historian SE
server.
4
Tag Explorer
Displays tags from Asset Framework and Data Archive.
5
Trend
Displays data from one or more tags, also known as traces, over a period of time.
6
Tag List
Displays the list of tags that are currently on the trend.