Display static value

The static value is a reference line for you to compare tag values. Ensure that at least one tag is displayed on the canvas, or the Static Value icon is disabled.
To display static value
  1. On the WebTrend toolbar, select
    Static Value
    (Static value).
  2. Select Add static value.
  3. Enter a name (optional) and a value.
  4. Select Save static value.
    Each tag can have multiple static values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal