GetServers
Retrieve the FactoryTalk Historian servers (Data Archive) that are connected to the API server.
Input Parameter
Item | Description |
|---|---|
Request | GET |
URL Parameter | None |
Request Header | Authentication : String (required). Bearer Token string returned from the Login action. |
Request Body | None |
Status Code |
|
Sample
Request Header
"Authorization": "eyJhbGciOiJIUzI1N…"
Response Body
{ "Result": [{ "ServerName": "HisSrvName", "ServerHost": "HisSrvHost" }], "Success": true, "ErrorMessage": "" }
Provide Feedback