CreateServerDigitalSets
Create the digital states in the specified FactoryTalk Historian server (Data Archive).
Input Parameter
Item | Description |
|---|---|
Request | POST |
URL Parameter | None |
Request Header | Authentication : String (required). Bearer Token string returned from the Login action. |
Request Body |
|
Status Code |
|
Sample
Request Header
"Authorization": "eyJhbGciOiJIUzI1N…"
Request Body
{"ServerName":"HisSrvName","DigitalSets":{"Digital1":["Success","Unknown"],"Digital2":["High","Low"]}}
Response Body
{ "Result": true, "Success": true, "ErrorMessage": "" }
Provide Feedback