Prerequisites

Ensure that following items are available to install Edge Operating System (Edge OS) into Edge Node:
  1. Edge node
  2. Monitor/TV
  3. USB keyboard
  4. USB stick (minimum recommended storage of 1 GB)
  5. VGA/HDMI cable connected to the monitor
  6. System to perform the installation transfer.
  7. Etcher Tool to flash the Edge Operating System (Edge OS) image on a USB.
  8. Latest Edge Operating System (Edge OS) RAW image file from PCDC (https://compatibility.rockwellautomation.com/Pages/home.aspx).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal