System explorer
Use the pane to view the contents of your project. The
System
explorerSystem
explorer contains the FactoryTalk Smart Object
s of your system. Under each FactoryTalk Smart Object
you create the program and routine with tags and parameters created for the FactoryTalk Smart Object
You can add programs, routines, and program or routine-scoped tags and parameters to FactoryTalk Smart Objects.
To open the System explorer, on the explorer bar, select
System
.Provide Feedback