Supported Fields for the Sequences Table
The following table provides the supported fields for the Sequences table:
Column Name | Column Type | Description | Example |
|---|---|---|---|
id | bigint | Unique Cognite provided identifier for the sequence. | 454501654069443 |
createdTime | timestamp | Time when this sequence was created in CDF in milliseconds since Jan 1, 1970. | 2019-09-07T15:50+00Z |
lastUpdatedTime | timestamp | Time when this sequence was updated in CDF in milliseconds since Jan 1, 1970. | 2019-09-07T15:50+00Z |
assetId | bigint | Optional asset this sequence is associated with. | 3039255880161656 |
name | varchar | Name of the sequence. | sequence_123 |
externalId | varchar | The external ID provided by the client. Must be unique for the resource type. | CDF_ExternalID |
description | varchar | The description of the sequence. | CDF project: testing_purpose |
dataSetId | bigint | Dataset this sequence belongs to. | 7166729101688251 |
Provide Feedback