Delete Invitation
Perform the following steps to delete a pending or an expired invitation:
- On the Management console, selectInvited Memberstab.
- Click the [
] icon in the Actionscolumn, against the email address for which you want to delete the invitation.Invited Members Listing
- ClickYesto confirm deleting the invitation andNootherwise.Delete Invite
The "Member invite deleted successfully" message is displayed.
Provide Feedback