Setting up Power BI Service using the Power BI Gateway
The steps for setting up Power BI Desktop are a pre-requisite for setting up a gateway connection.
Perform the following steps for setting up Power BI service using the Power BI gateway:
- Install the Power BI data gateway (standard mode or personal mode) application in your system.TIP:Click here to download the Power BI on-premises data gateway.
- Open the Power BI data gateway (standard mode or personal mode) application.PowerBI Gateway

- In the left menu, click theConnectorstab.
- In theLoad custom data connectors from the folderfield, provide the exact location of the downloaded connector file (DataMosaix.mez).
- ClickApply.
- In the dialog box, clickApply & Restartto apply the changes.After the restart, you will be able to view the updated connector file in the Connectors tab.
Provide Feedback