Conventions
The following conventions are followed in this document:
- Text, labels, and icon names are in bold. For example,End User License Agreementsscreen.
- Button names that appear in the user interface appear in square brackets. For example: Click [Start Import].
- Placeholder text for variable values appears in angled brackets with text in italics. For example: https://<hostname>:8090/<install folder>.
- The URLs and links appear in blue text. For example:https://www.rockwellautomation.com
- The cross-references appear in Green text. For example: Refer to“Plotting Data”.
Provide Feedback