Status bar
The status bar at the bottom of the Editor window usually displays a text message or state on the left side and the standard Caps Lock, Scroll Lock, and Num Lock states on the right side. In addition, to the immediate left of the Num Lock state, the status bar may display one or more icons representing the state and status of the Editor and/or its data.The following is a list of states that may be displayed in the status bar:
Icon | Item | Description |
![]() | Database | The Editor is accessing data. |
![]() | Error | An error occurred when editing data. |
![]() | Information | The currently selected data is predefined and not editable. |
![]() | Warning | A message displays a warning. |
![]() | Critical | A message displays critical error information. |
![]() | Question | A message displays a question. |
![]() | Searching | The Editor is searching for data. |
![]() | Secured | The currently selected data is secured. |
![]() | Printing | A report is being printed or previewed. |
![]() | Processing | The Editor is processing data. |
![]() | Waiting | The Editor is busy. |
![]() | Verification | Data is being verified. |
Provide Feedback