Menu bar
The menu bar is similar to the standard menu bar found on most Windows applications. The menu bar contains the drop-down menus for
File
, Edit
, View
, Tools
, and Help
.
This table describes the menu bar commands:
Item | Definition |
---|---|
File | Provides options for creating new objects, printing objects, and exiting the Editor. |
Edit | Provides options for deleting selected items and viewing item properties. You use the Properties option for editing various items. |
View | Allows you to show or hide the toolbar and status bar. You can also specify how data is viewed in the Detail pane and set user preferences for the Editor. |
Tools | Allows you to configure system properties. |
Help | Provides you with on-line help and information regarding the software and the system. |
Provide Feedback