List view
The List View mode of the Detail pane contains data items in a columnar or icon format, depending on the mode and selected item. There are four ways to display the data items in the List View (the associated toolbar button is seen to the left of each description):
Icon | Display | Description |
![]() | Large icons | Each item appears as a full-sized icon (32 x 32 pixels) with a label below it. You can drag the items to any location in the List View. |
![]() | Small icons | Each item appears as a small icon (16 x 16 pixels) with the label to the right of it. You can drag the items to any location in the List View. |
![]() | List | Each item appears as a small icon with a label to the right of it. Items are arranged in columns and cannot be dragged to any location in the List View. |
![]() | Details | Each item appears on its own line, with additional information arranged in columns to the right. The leftmost column contains the small icon and label, and subsequent columns contain subitems as specified by the Editor. |
With the exception of the first column of data in the List View, you cannot directly edit the data items. You can edit the data in the first column directly or right-click the desired item and select
Rename
.Provide Feedback