AfterLotInsert

Problem to be solved
This insertion point provides a way for the customer to initialize properties and attributes of a new lot. For example, the assignment of an initial lot state could involve a calculation of several variables. This insertion point provides a place to do this calculation to assign the correct lot state.
Specifics about this routine
This insertion interface is called after a new lot is created in the database, with the exception of a new lot created as the result of combining sublots of different lots in a composite container. These are the parameters to this function:
Param Name
Data Type
Description
LotName
String
Lot Name
CreationDate
Date
Creation Date of the Lot
MaterialID
Long
Material ID for the Material this Lot is derived
LotID
Long
Pkid of the Lot record in the database
This event is not fired for the insertion of a lot when a lot combination event occurs. In that event the
AfterCombinedLotInsert
event is fired. This event is only called when a plain generic insertion of Lot is performed.
Related insertion points
Other insertion points that could work with this function include:
  • AfterCombinedLotInsert
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal