Accessing the heel property from phase logic

The container heel property of a container supports being downloaded to phase logic. The 7800, 17800, 8000 and 18000 series phase requests to download data from the Material Database are used to download the heel property of any container.
The container heel property of a container supports being uploaded from phase logic. The 7800, 17800, 8000 and 18000 series phase requests to upload data from the Material Database are used to upload a value to the heel property of any container.
The 7800, 17800, 83NN, 183NN, 87NN and 187NN phase requests require an integer to identify the property to be referenced. For containers, the Heel Property will have an index of 10.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal