FactoryTalk Batch View
FactoryTalk Batch View
is a modern, browser-based interface that allows you to initiate and control the batch process anywhere there is an internet connection. The FactoryTalk Batch View
interface adapts across smartphones, such as iOS and Android, to tablets and PCs. Users can access real-time information and interact with their process from the plant floor to the production office.FactoryTalk Batch View
is well-suited for large industrial facilities that have workstation infrastructure limitations and require multiple access points across the plant. With personalized user profiles that are tailored to the user, such as language switching options, workers at different levels of the organization can stay mobile yet connected to their process operations.Key capabilities of the solution include:
- A modern web interface offers adaptation to new or existing platforms and environments with backward compatibility to previous versions ofFactoryTalk Batchsoftware; single-server architecture allows for new features and functions to be added with minimal impact to operations.
- Information-enabled and secure. Uses common system security policies for access control similar to any workstation, as a node on the plant network.
- Interfaces support multiple mobile devices and are easily integrated with HMI screens onto workstations.
Provide Feedback