UpdateStorageLocation
Updates a StorageLocation record in the material database.
Syntax
MaterialSvr
.
UpdateStorageLocation
(StorageLocation
As StorageLocation)The
UpdateStorageLocation
method syntax has these parts:Part | Description |
---|---|
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
StorageLocation | An instance of a StorageLocation object. |
Provide Feedback