UpdateErrorCorrection

Updates a QA error correction record associated with a test specification in the material database.
Syntax
MaterialSvr.UpdateErrorCorrection
(
ErrorCorrection
As ErrorCorrection)
The
UpdateErrorCorrection
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialSvr interface to which the method is directed.
ErrorCorrection
An instance of a ErrorCorrection object.
Remarks
This interface will allow for the modification of QA error correction records in the material database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal