UpdateContainerPriority

Updates a ContainerPriority record in the material database.
Syntax
MaterialSvr.UpdateContainerPriority
(
ContainerPriority
As ContainerPriority)
The
UpdateContainerPriority
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
ContainerPriority
An instance of a ContainerPriority object.
Remarks
The only property that can be updated in the ContainerPriority object is the ‘Priority’.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal