IsMaterialServerAvailable
Returns a Boolean value (TRUE or FALSE) indicating if there is communications to the Material Server.
Syntax
bResult
= MaterialServerUtils
.IsMaterialServerAvailable
()The
IsMaterialServerAvailable
method syntax has these parts:Part | Description |
---|---|
bResult | Boolean value that returns TRUE or FALSE which represents if the server successfully initialized all connection points. |
MaterialServerUtils | Instance of the MaterialServerUtils Interface to which the method is directed. |
Provide Feedback