InsertMaterial
Inserts a Material record into the material database.
Syntax
MaterialSvr
.InsertMaterial
(Material
As Material)The
InsertMaterial
method syntax has these parts:Part | Description |
MaterialSvr | Instance of the MaterialServer Interface to which the method is directed. |
Material | An instance of a Material object. |
Provide Feedback