InsertLotState

Inserts a Lot State record into the material database.
Syntax
MaterialSvr
.
InsertLotState
(
LotState
As LotState)
The
InsertLotState
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
LotState
An instance of a LotState object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal