InsertLot

Inserts a Lot record into the material database.
Syntax
Material
.
InsertLot
(
Lot
As Lot)
The
InsertLot
method syntax has these parts:
Part
Description
Material
Instance of a Material object to which the method is directed.
Lot
An instance of a Lot object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal