InsertLimit

Inserts a QA test specification limit record associated with a base test specification in the material database.
Syntax
TestSpecification
.
InsertLimit
(
TestSpecificationLimit
As TestSpecificationLimit)
The
InsertLimit
method syntax has these parts:
Part
Description
TestSpecification
Instance of the QATestSpec interface to which the method is directed.
TestSpecificationLimit
An instance of a TestSpecificationLimit object.
Remarks
This new interface will allow for the insertion of QA test specification limits to be associated with a test specification. The requirements state that a test specification can be composed of any number of material properties. Having limit sections allows for a one-to-many relationship.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal