InsertContainerState

Inserts a Container State record into the material database.
Syntax
MaterialSvr
.
InsertContainerState
(
ContainerState
As ContainerState)
The
InsertContainerState
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
ContainerState
An instance of a ContainerState object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal