InsertContainer

Inserts a Container record into the material database.
Syntax
MaterialSvr
.
InsertContainer
(
Container
As Container)
The
InsertContainer
method syntax has these parts:
Part
Description
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
Container
An instance of a Container object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal