GetStorageLocationByID

Returns a StorageLocation object with its properties populated with corresponding data from the material database, based on the StorageLocationID.
Syntax
Set
object
=
MaterialSvr
.
GetStorageLocationByID
(ByVal
IStorageLocationID
As Long)
The
GetStorageLocationByID
method syntax has these parts:
Part
Description
object
Reference to a valid StorageLocation object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
IStorageLocationID
Represents the ID of the StorageLocation.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal