GetMaterialTypeByID

Returns a MaterialType object with its properties populated with corresponding data from the material database, based on the MaterialTypeID.
Syntax
Set
object
=
MaterialSvr
.
GetMaterialTypeByID
(ByVal
MaterialTypeID
As Long)
The
GetMaterialTypeByID
method syntax has these parts:
Part
Description
object
Reference to a valid MaterialType object.
MaterialSvr
Instance of the MaterialServer Interface to which the method is directed.
MaterialTypeID
Represents the ID of the MaterialType.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal